Event: DCD Connect | London, September 16-17 Read more

Data Center Technologies

Liquid Cooling for Data Centers

AI, HPC, and next-generation compute loads are pushing heat densities beyond the limits of air cooling. Liquid cooling removes heat at the source, enabling higher rack densities, lower PUE, and stable performance.

Validate the right hybrid or liquid-cooled architecture with Munters experts.

A Munters technician wearing safety glasses and a gray work vest, applying protective wrap to a large cylindrical component of an industrial chiller system.
A close-up photograph of a technician's hands in dark, textured work gloves, using a tool to adjust or wire a row of green and gray electrical terminal blocks inside a control panel for a cooling system.

Liquid Cooling Solutions

Liquid cooling is the foundation of modern infrastructure

It has evolved into the mandatory standard for high-density deployments, providing the thermal headroom required for next-generation compute.

Why Data Centers are Shifting to Liquid Cooling

The move toward liquid cooling is driven by rising compute intensity and energy demands. Modern facilities choose liquid cooling because it delivers:

  • Stable cooling for high-density, high transient AI and HPC loads
  • Lower PUE and sharply reduced fan power
  • Greater rack density per square foot
  • Improved reliability in high-ambient, water-constrained or space-constrained environments
  • Flexibility for hybrid air-and-liquid deployments
  • A clear upgrade path for next generation GPU and CPU roadmaps
  • Seamless coexistence with air cooling to protect diverse hardware types across the white space

Liquid cooling technologies explained

Data centers use different liquid cooling approaches depending on density, architectures and operational need. The most common options include:

  • Direct-to-chip liquid cooling

    Single phase

    Liquid circulates through cold plates attached to CPUs and GPUs, removing heat directly at the source. Ideal for dense AI and HPC racks.

    Two-phase

    Refrigerant or dielectric fluid evaporates at the cold plate and condenses elsewhere in the loop. Delivers maxium efficiency for ultra high density compute.

    A close-up, stylized graphic of a blue printed circuit board featuring two prominent computer processors and intricate golden circuit pathways, representing direct-to-chip liquid cooling targets.
  • Liquid-to-liquid CDUs (LCX)

    Munters LCX transfer heat from the server-side liquid loop to a facility water loop (chilled or elevated-temperature), while providing pumping, pressure control, filtration and a temperature regulation.

    Used with chillers, dry coolers or free-cooling systems in standard liquid-cooling deployments.

    Product rendering of a dark gray Munters LCX coolant distribution unit (CDU) cabinet, shown with an open access panel revealing the internal pumps, piping, and filtration components designed for liquid-to-liquid data center cooling.
  • Liquid to refrigerant CDUs (SyCool LCE)

    Transfers heat to a refrigerant thermosyphon instead of chilled water. Enables fully water free liquid cooling for sites with water constraints.

    A 3D product rendering of a dark gray, rectangular Munters SyCool LCE Coolant Distribution Unit (CDU) cabinet with piping connection ports protruding from its top surface, isolated on a light gray background.
  • Rear-door heat exchangers

    Capture heat at the rack using liquid coils mounted in the rear door. Useful for retrofits or as a transition toward full liquid cooling.

    A 3D diagrammatic rendering of a server rack cabinet illustrating a rear-door heat exchanger panel with cooling coils detached from the back of the rack to showcase the thermal management design.
  • Hybrid liquid + air cooling

    Combines traditional air cooling with targeted liquid cooling for high density racks

    Allows gradual adoption within existing facilities

    A multi-story technical 3D rendering of a hybrid data center cooling system, showing a Munters Geoclima 2MW chiller on the roof connected via liquid piping to an LCX-500 coolant distribution unit and a Modular Chilled Wall 350 system.

Choose liquid cooling when

Heat density, efficiency or space constraints push beyond what air can reliably handle.

Note on Hybrid Environments: Choosing liquid cooling does not require abandoning air cooling. Most modern high-density facilities operate as hybrid environments, leveraging Munters CDUs to manage high-TDP AI clusters while existing CRAH or fan wall systems continue to handle the room’s ambient heat and lower-density racks.

  • Rack densities exceed traditional limits
  • AI, GPU or HPC clusters create rapid load swings
  • Efficiency and low PUE are critical
  • High ambient temperatures limit air cooling
  • Floor space is constrained
  • Noise reduction matters
  • Water usage must be minimized (refrigerant based systems)
  • Heat recovery for district heating is a priority

Choose air cooling when

Simplicity, cost control and moderate densities are the primary goals.

  • Density is moderate
  • Flexibility and simplicity are priorities
  • Existing infrastructure supports growth

Munters LCX CDU, engineered liquid cooling for data center environments

The LCX is Munters liquid-to-liquid CDU for mission-critical data centers, delivering efficient heat transfer, precise coolant control and high reliability across dynamic AI and high-density workloads. It enables a smooth transition from CRAH-based air cooling to scalable liquid-cooled architectures, from initial AI racks to fully liquid-cooled white spaces.

Key characteristics include:

  • Liquid-to-liquid heat exchange for high transfer efficiency and stable coolant temperatures

  • Modular and scalable architecture for expansion and flexible deployment

  • Compatibility with single-phase and dielectric liquid cooling, including advanced direct-to-chip systems

  • Perfect pairing with Munters chillers for integrated cooling loops

  • Upgrade path from air cooling to liquid cooling for existing facilities

  • High-efficiency heat exchangers for stable performance across wide delta-T ranges

  • Sensor-driven monitoring of flow, pressure and temperature for precise control

  • Integration with BMS and DCS platforms

  • N+1 and N+N pump redundancy for uninterrupted operation

  • Support for high-density racks, AI clusters and HPC deployments

A 3D diagrammatic cutaway rendering of a data center showcasing the Munters SyCool LCE refrigerant-based liquid cooling system, illustrating roof-mounted heat rejection units connected by vertical piping to indoor cabinets and server racks with blue and red arrows representing thermal airflow and liquid cooling loops.

Munters SyCool LCE – refrigerant-based liquid cooling

For water-free or refrigerant-based cooling strategies. Munters offers SyCool LCE, a liquid-to-refrigerant CDU designed for thermosiphon architectures.

  • Completely water-free operation
  • High efficiency and low maintenance through thermosyphon technology
  • Compatibility with refrigerant-based racks and next-generation direct-to-chip systems
  • A conversion path from air cooling to liquid cooling in SyCool deployments

Industry trends shaping liquid cooling adoption

Several macro trends are acceleration the shift from air to liquid cooling across the data center industry.

As a result, liquid cooling is rapidly becoming the default architecture for high-performance compute.

For a deeper look at GPU density, AI workloads and future thermal requirements, explore our AI data center cooling guidance.

  • Explosive AI and HPC growth driving extreme rack densities
  • Rising CPU and GPU thermal design power (TDP)
  • Sustainability targets and lower PUE requirements
  • Water scarcity and stricter water-use regulations
  • Space constraints in colocation and urban facilities
  • Demand for quieter, smaller and more energy-efficient footprints
  • Enables higher supply temperatures and greater use of free cooling

Challenges and future outlook for liquid cooling

Liquid cooling introduces new operational considerations for data center teams.

Munters addresses these challenges through engineered systems, built-in redundancy, advanced monitoring and lifecycle support.

As AI and high-density compute continue to grow, liquid cooling will move from optional to essential.

Common challenges include:

  • Leak management and monitoring
  • Safe fluid handling and coolant compatibility
  • Integration with existing air-cooled systems
  • Controls complexity
  • Installation and commissioning requirements
  • Staff training
Two technicians in gray work vests and safety glasses working on the open electrical cabinet of a large industrial Munters cooling unit, inspecting the internal wiring and control panel.

What liquid cooling is and how it works

Liquid cooling removes heat directly at the source inside the server or rack using chilled water or dielectric fluids. The process typically follows these steps:

  • Cold liquid is delivered to cold plates or in server heat exchangers.
  • Heat is absorbed from CPUs, GPUs and other accelerators.
  • Warm liquid returns to a CDU for pressure, flow, temperature control and filtration.
  • The CDU transfers this heat to the facility cooling loop for rejection through a chiller, dry cooler or into heat-reuse systems.
  • Cooled liquid is circulated back to the rack to repeat the cycle.

FAQ – liquid cooling in data centers

A smiling Munters technician wearing safety glasses and work gloves, using a power drill to assemble a metal frame structure inside a manufacturing facility.

Ready to explore liquid cooling? Let us demonstrate how Munters liquid cooling systems can support AI-ready performance, efficiency and scalability in your data center.